SNVSC75B April 2023 – September 2025 LM5171-Q1
PRODUCTION DATA
Each channel of the LM5171-Q1 has a robust 5A (peak) half bridge driver to drive external N-channel power MOSFETs. As shown in Figure 6-16, the low-side drive is directly powered by VCC, and the high-side driver by the bootstrap capacitor CBT. During the on-time of the low-side driver, the SW pin is pulled down to PGND and CBT is charged by VCC through the boot diode DBT. TI recommends selecting a 0.1µF or larger ceramic capacitor for CBT, and an ultra-fast diode of 1A and 100V ratings for DBT. TI also strongly recommends users to add a 2Ω to 5Ω resistor (RBT) in series with DBT to limit the surge charging current and improve the noise immunity of the high-side driver.
In case during start-up in buck mode, CBT is not charged initially; the LM5171-Q1 then holds off the high-side driver outputs (HO1 and HO2) and sends LO pulses of 100ns width in consecutive cycles to pre-charge CBT. When the boot voltage is greater than the 6.5V boot UV threshold, the high-side drivers output PWM signals at the HO1 and HO2 pins for normal switching action. If the boot voltage becomes lower than the boot UV threshold voltage on the falling edge, the corresponding HO output pulls low until the boot voltage recovers to assume normal HO switching pulses. During normal buck mode operation, when the CBT voltage falls below the 6.5V boot UV threshold, the same precharge function starts by interrupting the normal switching until the boot voltage restores above the UV threshold. The pre-charge function helps prevent the power MOSFETs from running into linear mode by inadequate gate voltage. Note that the gate threshold voltage of the MOSFETs potentially rises to 6V due to degradation over aging.
During start-up and normal operation in boost mode, CBT is naturally charged by the normal turn on of the low side MOSFET, therefore there is no such 100-ns pre-charge pulse at the LO pins.
To prevent shoot-through between the high-side and low-side power MOSFETs on the same half bridge leg, two types of dead time schemes are selected with the DT pin: the programmable dead time or built-in adaptive dead time.
To program the dead time, place a resistor RDT across the DT/SD and AGND pins as shown in Figure 6-17.
The dead time tDT as depicted in Figure 6-18 is determined by Equation 12:
Note that the equation is valid for programming tDT between 15ns and 200ns. When the power MOSFET is connected to the gate drive, its gate input capacitance CISS becomes a load of the gate drive output, and the HO and LO slew rate are reduced, leading to a reduced effective tDT between the high- and low-side MOSFETs. Evaluate the effective tDT to make sure it is adequate to prevent shoot-through between the high- and low-side MOSFETs.
When the DT programmability is not used, simply connect the DT/SD pin to VDD as shown in Figure 6-19, to activate the built-in adaptive dead time. The adaptive dead time is implemented by real time monitoring of the output of a driver (either HO or LO) by the other driver (LO or HO) of the same half bridge switch leg, as shown in Figure 6-19 and Figure 6-20. Only when the output voltage of a driver falls below 1.5V does the other driver starts turn on. The effectiveness of adaptive dead time is greatly reduced if a series gate resistor is used, or if the PCB traces of the gate drive have excessive impedance due to poor layout design.