SNVSC75B April 2023 – September 2025 LM5171-Q1
PRODUCTION DATA
TI recommends setting a hard limit for the ISETx signal such that the converter is not over driven by an errant current setting signal. Assume the converter is allowed up to 10% overloading current. Refer to Channel Current Setting Commands (ISET1 and ISET2), the analog current setting signal ISETx needs to be limited by the following voltage level:
As shown in Figure 8-6, RISETT and RISETB are used to limit the maximum voltage on ISETx.
TLV431 or op amp are used to clamp the ISETx voltage in a precise way as shown in ISET Clamp.