Equation 29 indicates that the power plant is basically a first-order system. A Type-II compensator
as shown in Figure 8-1 is adequate to stabilize the loop for both buck and boost mode operations.
Assuming the output impedance of the gm
amplifier is RGM, the current loop compensation gain is determined by :
Equation 30.
where
- ACS is the current sense
amplifier gain, that is 40;
- Gm is the trans-conductance of the gm error amplifier, which
is 100μA/V;
- ZCOMP(s) is the equivalent impedance of the compensation
network seen at the COMP pin (see Figure 8-1)
Equation 31.
Considering CHF <<
CCOMP, Equation 31 is simplified to :
Equation 32.
Because RGM is > 5MegΩ, and
the frequency range for loop compensation is usually above a few kHz, the effects of
RGM on the loop gain in the interested frequency range becomes negligible.
Therefore, substituting Equation 32 into Equation 30, and neglecting RGM,
Equation 33.
From Figure 8-2, the open-loop gain of the inner current loop is:
Equation 34.
where
Equation 35.
Equation 36.
- KFF is the ramp generator
coefficient. For LM5171-Q1, KFF=0.03125.
Substituting Equation 33 and Equation 29 into Equation 34, Ti(s) is found as:
Equation 37.
The poles and zeros of the total loop
transfer function are determined by:
Equation 38.
Equation 39.
Equation 40.
To tailor the total inner current loop gain
to crossover at fCI, select the components of the compensation network according
to the following guidelines, then fine tune the network for optimal loop performance.
- The zero fz is placed at
around 1/5 of target crossover frequency fCI,
- The pole fp2 is placed at
approximately 1/2 of switching frequency fSW,
- The total open-loop gain is set to
unity at fCI, namely,
Equation 41.
Therefore, the compensation components are
derived from the above equations, as shown in Equation 42.
Equation 42.