SPRY303F May 2019 – February 2025 AM3351 , AM3352 , AM3354 , AM3356 , AM3357 , AM3358 , AM3358-EP , AM3359 , AM4372 , AM4376 , AM4377 , AM4378 , AM4379 , AM5706 , AM5708 , AM5746 , AM5748 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62L , AM62P , AM62P-Q1 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442 , AM6526 , AM6528 , AM6546 , AM6548 , AM68 , AM68A , AM69 , AM69A , DRA821U , DRA821U-Q1 , DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
In order to trust communications over a local-area network (LAN), wide-area network (WAN) or the Internet, devices must have a unique identity which can be shared. Communicating devices can then decide the authenticity or trustworthiness of the other devices participating in the conversation.
Application processors often come with a unique identification (ID) code of some sort. Alternatively, or in addition to the ID code, devices might identify themselves through a signature or certificate key with a corresponding public key that is accessible through a cloud service, for example.
Figure 2 Device ID helps prevent
theft.