SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Table 20-135 lists the memory-mapped registers for the AUX_TIMER2 registers. All register offset addresses not listed in Table 20-135 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Section |
|---|---|---|---|
| 0h | CTL | Timer Control | Section 20.8.7.1 |
| 4h | TARGET | Target | Section 20.8.7.2 |
| 8h | SHDWTARGET | Shadow Target | Section 20.8.7.3 |
| Ch | CNTR | Counter | Section 20.8.7.4 |
| 10h | PRECFG | Clock Prescaler Configuration | Section 20.8.7.5 |
| 14h | EVCTL | Event Control | Section 20.8.7.6 |
| 18h | PULSETRIG | Pulse Trigger | Section 20.8.7.7 |
| 80h | CH0EVCFG | Channel 0 Event Configuration | Section 20.8.7.8 |
| 84h | CH0CCFG | Channel 0 Capture Configuration | Section 20.8.7.9 |
| 88h | CH0PCC | Channel 0 Pipeline Capture Compare | Section 20.8.7.10 |
| 8Ch | CH0CC | Channel 0 Capture Compare | Section 20.8.7.11 |
| 90h | CH1EVCFG | Channel 1 Event Configuration | Section 20.8.7.12 |
| 94h | CH1CCFG | Channel 1 Capture Configuration | Section 20.8.7.13 |
| 98h | CH1PCC | Channel 1 Pipeline Capture Compare | Section 20.8.7.14 |
| 9Ch | CH1CC | Channel 1 Capture Compare | Section 20.8.7.15 |
| A0h | CH2EVCFG | Channel 2 Event Configuration | Section 20.8.7.16 |
| A4h | CH2CCFG | Channel 2 Capture Configuration | Section 20.8.7.17 |
| A8h | CH2PCC | Channel 2 Pipeline Capture Compare | Section 20.8.7.18 |
| ACh | CH2CC | Channel 2 Capture Compare | Section 20.8.7.19 |
| B0h | CH3EVCFG | Channel 3 Event Configuration | Section 20.8.7.20 |
| B4h | CH3CCFG | Channel 3 Capture Configuration | Section 20.8.7.21 |
| B8h | CH3PCC | Channel 3 Pipeline Capture Compare | Section 20.8.7.22 |
| BCh | CH3CC | Channel 3 Capture Compare | Section 20.8.7.23 |
Complex bit access types are encoded to fit into small table cells. Table 20-136 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
CTL is shown in Table 20-137.
Return to the Summary Table.
Timer Control
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-7 | RESERVED | R | 0h | Reserved |
| 6 | CH3_RESET | R/W | 0h | Channel 3 reset. 0: No effect. 1: Reset CH3CC, CH3PCC, CH3EVCFG, and CH3CCFG. Read returns 0. |
| 5 | CH2_RESET | R/W | 0h | Channel 2 reset. 0: No effect. 1: Reset CH2CC, CH2PCC, CH2EVCFG, and CH2CCFG. Read returns 0. |
| 4 | CH1_RESET | R/W | 0h | Channel 1 reset. 0: No effect. 1: Reset CH1CC, CH1PCC, CH1EVCFG, and CH1CCFG. Read returns 0. |
| 3 | CH0_RESET | R/W | 0h | Channel 0 reset. 0: No effect. 1: Reset CH0CC, CH0PCC, CH0EVCFG, and CH0CCFG. Read returns 0. |
| 2 | TARGET_EN | R/W | 0h | Select counter target value. You must select TARGET to use shadow target functionality. 0h = 65535 1h = TARGET.VALUE |
| 1-0 | MODE | R/W | 0h | Timer mode control. The timer restarts from 0 when you set MODE to UP_ONCE, UP_PER, or UPDWN_PER. When you write MODE all internally queued updates to [CHnCC.*] and TARGET clear. 0h = Disable timer. Updates to counter, channels, and events stop. 1h = Count up once. The timer increments from 0 to target value, then stops and sets MODE to DIS. 2h = Count up periodically. The timer increments from 0 to target value, repeatedly. Period = (target value + 1) * timer clock period 3h = Count up and down periodically. The timer counts from 0 to target value and back to 0, repeatedly. Period = (target value * 2) * timer clock period |
TARGET is shown in Table 20-138.
Return to the Summary Table.
Target
User defined counter target.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | 16 bit user defined counter target value, which is used when selected by CTL.TARGET_EN. |
SHDWTARGET is shown in Table 20-139.
Return to the Summary Table.
Shadow Target
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Target value for next counter period. The timer copies VALUE to TARGET.VALUE when CNTR.VALUE becomes 0. The copy does not happen when you restart the timer. This is useful to avoid period jitter in PWM applications with time-varying period, sometimes referenced as phase corrected PWM. |
CNTR is shown in Table 20-140.
Return to the Summary Table.
Counter
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R | 0h | 16 bit current counter value. |
PRECFG is shown in Table 20-141.
Return to the Summary Table.
Clock Prescaler Configuration
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7-0 | CLKDIV | R/W | 0h | Clock division. CLKDIV determines the timer clock frequency for counter, synchronization, and timer event updates. The timer clock frequency is the clock selected by AUX_SYSIF:TIMER2CLKCTL.SRC divided by (CLKDIV + 1). This inverse is the timer clock period. 0x00: Divide by 1. 0x01: Divide by 2. ... 0xFF: Divide by 256. |
EVCTL is shown in Table 20-142.
Return to the Summary Table.
Event Control
Set and clear individual events manually. Manual update of an event takes priority over automatic channel updates to the same event. You cannot set and clear an event at the same time, such requests will be neglected.
An event can be automatically cleared, set, toggled, or pulsed by each channel, listed in decreasing order of priority. The action with highest priority happens when multiple channels want to update an event at the same time.
The four events connect to the asynchronous AUX event bus:
- Event 0 connects to AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0.
- Event 1 connects to AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1.
- Event 2 connects to AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2.
- Event 3 connects to AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | EV3_SET | W | 0h | Set event 3. Write 1 to set event 3. |
| 6 | EV3_CLR | W | 0h | Clear event 3. Write 1 to clear event 3. |
| 5 | EV2_SET | W | 0h | Set event 2. Write 1 to set event 2. |
| 4 | EV2_CLR | W | 0h | Clear event 2. Write 1 to clear event 2. |
| 3 | EV1_SET | W | 0h | Set event 1. Write 1 to set event 1. |
| 2 | EV1_CLR | W | 0h | Clear event 1. Write 1 to clear event 1. |
| 1 | EV0_SET | W | 0h | Set event 0. Write 1 to set event 0. |
| 0 | EV0_CLR | W | 0h | Clear event 0. Write 1 to clear event 0. |
PULSETRIG is shown in Table 20-143.
Return to the Summary Table.
Pulse Trigger
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | TRIG | W | 0h | Pulse trigger. Write 1 to generate a pulse to AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE. Pulse width equals the duty cycle of AUX_SYSIF:TIMER2CLKCTL.SRC. |
CH0EVCFG is shown in Table 20-144.
Return to the Summary Table.
Channel 0 Event Configuration
This register configures channel function and enables event outputs.
Each channel has an edge-detection circuit with memory. The circuit is:
- enabled while CCACT selects a capture function and CTL.MODE is different from DIS.
- flushed while CCACT selects a capture function and you change CTL.MODE from DIS to another mode.
The flush action uses two AUX_SYSIF:TIMER2CLKCTL.SRC clock periods. It prevents capture events caused by expired signal values stored in the edge-detection circuit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | EV3_GEN | R/W | 0h | Event 3 enable. 0: Channel 0 does not control event 3. 1: Channel 0 controls event 3. When 0 < CCACT < 8, EV3_GEN becomes zero after a capture or compare event. |
| 6 | EV2_GEN | R/W | 0h | Event 2 enable. 0: Channel 0 does not control event 2. 1: Channel 0 controls event 2. When 0 < CCACT < 8, EV2_GEN becomes zero after a capture or compare event. |
| 5 | EV1_GEN | R/W | 0h | Event 1 enable. 0: Channel 0 does not control event 1. 1: Channel 0 controls event 1. When 0 < CCACT < 8, EV1_GEN becomes zero after a capture or compare event. |
| 4 | EV0_GEN | R/W | 0h | Event 0 enable. 0: Channel 0 does not control event 0. 1: Channel 0 controls event 0. When 0 < CCACT < 8, EV0_GEN becomes zero after a capture or compare event. |
| 3-0 | CCACT | R/W | 0h | Capture-Compare action. Capture-Compare action defines 15 different channel functions that utilize capture, compare, and zero events. 0h = Disable channel. 1h = Set on capture, and then disable channel. Channel function sequence: - Set enabled events on capture event and copy CNTR.VALUE to CH0CC.VALUE. - Disable channel. Primary use scenario is to select this function before you start the timer. Follow these steps if you need to select this function while CTL.MODE is different from DIS: - Set CCACT to SET_ON_CAPT with no event enable. - Configure CH0CCFG (optional). - Wait for three timer clock periods as defined in PRECFG before you set CCACT to SET_ON_CAPT_DIS. Event enable is optional. These steps prevent capture events caused by expired signal values in edge-detection circuit. 2h = Clear on zero, toggle on compare, and then disable channel. Channel function sequence: - Clear enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH0CC.VALUE = CNTR.VALUE. - Disable channel. Enabled events are set when CH0CC.VALUE = 0 and CNTR.VALUE = 0. 3h = Set on zero, toggle on compare, and then disable channel. Channel function sequence: - Set enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH0CC.VALUE = CNTR.VALUE. - Disable channel. Enabled events are cleared when CH0CC.VALUE = 0 and CNTR.VALUE = 0. 4h = Clear on compare, and then disable channel. Channel function sequence: - Clear enabled events when CH0CC.VALUE = CNTR.VALUE. - Disable channel. 5h = Set on compare, and then disable channel. Channel function sequence: - Set enabled events when CH0CC.VALUE = CNTR.VALUE. - Disable channel. 6h = Toggle on compare, and then disable channel. Channel function sequence: - Toggle enabled events when CH0CC.VALUE = CNTR.VALUE. - Disable channel. 7h = Pulse on compare, and then disable channel. Channel function sequence: - Pulse enabled events when CH0CC.VALUE = CNTR.VALUE. - Disable channel. The event is high for two timer clock periods. 8h = Period and pulse width measurement. Continuously capture period and pulse width of the signal selected by CH0CCFG.CAPT_SRC relative to the signal edge given by CH0CCFG.EDGE. Set enabled events when CH0CC.VALUE contains signal period and CH0PCC.VALUE contains signal pulse width. Notes: - Make sure that you configure CH0CCFG.CAPT_SRC and CCACT when CTL.MODE equals DIS, then set CTL.MODE to UP_ONCE or UP_PER. - The counter restarts in the selected timer mode when CH0CC.VALUE contains the signal period. - If more than one channel uses this function, the channels will perform this function one at a time. The channel with lowest number has priority and performs the function first. Next measurement starts when current measurement completes successfully or times out. A timeout occurs when counter equals target. - If you want to observe a timeout event configure another channel to SET_ON_CAPT. Signal property requirements: - Signal Period >= 2 * ( 1 + PRECFG.CLKDIV ) * timer clock period. - Signal Period <= 65535 * (1 + PRECFG.CLKDIV ) * timer clock period. - Signal low and high phase >= (1 + PRECFG.CLKDIV ) * timer clock period. 9h = Set on capture repeatedly. Channel function sequence: - Set enabled events on capture event and copy CNTR.VALUE to CH0CC.VALUE. Primary use scenario is to select this function before you start the timer. Follow these steps if you need to select this function while CTL.MODE is different from DIS: - Select this function with no event enable. - Configure CH0CCFG (optional). - Wait for three timer clock periods as defined in PRECFG before you enable events. These steps prevent capture events caused by expired signal values in edge-detection circuit. Ah = Clear on zero, toggle on compare repeatedly. Channel function sequence: - Clear enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH0CC.VALUE = CNTR.VALUE. Set CTL.MODE to UPDWN_PER for center-aligned PWM generation. Duty cycle is given by: When CH0CC.VALUE <= TARGET.VALUE: Duty cycle = 1 - ( CH0CC.VALUE / TARGET.VALUE ). When CH0CC.VALUE > TARGET.VALUE: Duty cycle = 0. Enabled events are set when CH0CC.VALUE = 0 and CNTR.VALUE = 0. Bh = Set on zero, toggle on compare repeatedly. Channel function sequence: - Set enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH0CC.VALUE = CNTR.VALUE. Set CTL.MODE to UP_PER for edge-aligned PWM generation. Duty cycle is given by: When CH0CC.VALUE <= TARGET.VALUE: Duty cycle = CH0CC.VALUE / ( TARGET.VALUE + 1 ). When CH0CC.VALUE > TARGET.VALUE: Duty cycle = 1. Enabled events are cleared when CH0CC.VALUE = 0 and CNTR.VALUE = 0. Ch = Clear on compare repeatedly. Channel function sequence: - Clear enabled events when CH0CC.VALUE = CNTR.VALUE. Dh = Set on compare repeatedly. Channel function sequence: - Set enabled events when CH0CC.VALUE = CNTR.VALUE. Eh = Toggle on compare repeatedly. Channel function sequence: - Toggle enabled events when CH0CC.VALUE = CNTR.VALUE. Fh = Pulse on compare repeatedly. Channel function sequence: - Pulse enabled events when CH0CC.VALUE = CNTR.VALUE. The event is high for two timer clock periods. |
CH0CCFG is shown in Table 20-145.
Return to the Summary Table.
Channel 0 Capture Configuration
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-7 | RESERVED | R | 0h | Reserved |
| 6-1 | CAPT_SRC | R/W | 0h | Select capture signal source from the asynchronous AUX event bus. The selected signal enters the edge-detection circuit. False capture events can occur when: - the edge-detection circuit contains expired signal samples and the circuit is enabled without flush as described in CH0EVCFG - this register is reconfigured while CTL.MODE is different from DIS. You can avoid false capture events. When wanted channel function is: - SET_ON_CAPT_DIS, see description for SET_ON_CAPT_DIS in CH0EVCFG.CCACT. - SET_ON_CAPT, see description for SET_ON_CAPT in CH0EVCFG.CCACT. - PER_PULSE_WIDTH_MEAS, see description for PER_PULSE_WIDTH_MEAS in CH0EVCFG.CCACT. If you write a non-enumerated value the behavior is identical to NO_EVENT. The written value is returned when read. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
| 0 | EDGE | R/W | 0h | Edge configuration. Channel captures counter value at selected edge on signal source selected by CAPT_SRC. See CH0EVCFG.CCACT. 0h = Capture CNTR.VALUE at falling edge of CAPT_SRC. 1h = Capture CNTR.VALUE at rising edge of CAPT_SRC. |
CH0PCC is shown in Table 20-146.
Return to the Summary Table.
Channel 0 Pipeline Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Pipeline Capture Compare value. 16-bit user defined pipeline compare value or channel-updated capture value. Compare mode: An update of VALUE will be transferred to CH0CC.VALUE when the next CNTR.VALUE is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When CH0EVCFG.CCACT equals PER_PULSE_WIDTH_MEAS then VALUE contains the width of the low or high phase of the selected signal. This is specified by CH0CCFG.EDGE and CH0CCFG.CAPT_SRC. |
CH0CC is shown in Table 20-147.
Return to the Summary Table.
Channel 0 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Capture Compare value. 16-bit user defined compare value or channel-updated capture value. Compare mode: VALUE is compared against CNTR.VALUE and an event is generated as specified by CH0EVCFG.CCACT when these are equal. Capture mode: The current counter value is stored in VALUE when a capture event occurs. CH0EVCFG.CCACT determines if VALUE is a signal period or a regular capture value. |
CH1EVCFG is shown in Table 20-148.
Return to the Summary Table.
Channel 1 Event Configuration
This register configures channel function and enables event outputs.
Each channel has an edge-detection circuit with memory. The circuit is:
- enabled while CCACT selects a capture function and CTL.MODE is different from DIS.
- flushed while CCACT selects a capture function and you change CTL.MODE from DIS to another mode.
The flush action uses two AUX_SYSIF:TIMER2CLKCTL.SRC clock periods. It prevents capture events caused by expired signal values stored in the edge-detection circuit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | EV3_GEN | R/W | 0h | Event 3 enable. 0: Channel 1 does not control event 3. 1: Channel 1 controls event 3. When 0 < CCACT < 8, EV3_GEN becomes zero after a capture or compare event. |
| 6 | EV2_GEN | R/W | 0h | Event 2 enable. 0: Channel 1 does not control event 2. 1: Channel 1 controls event 2. When 0 < CCACT < 8, EV2_GEN becomes zero after a capture or compare event. |
| 5 | EV1_GEN | R/W | 0h | Event 1 enable. 0: Channel 1 does not control event 1. 1: Channel 1 controls event 1. When 0 < CCACT < 8, EV1_GEN becomes zero after a capture or compare event. |
| 4 | EV0_GEN | R/W | 0h | Event 0 enable. 0: Channel 1 does not control event 0. 1: Channel 1 controls event 0. When 0 < CCACT < 8, EV0_GEN becomes zero after a capture or compare event. |
| 3-0 | CCACT | R/W | 0h | Capture-Compare action. Capture-Compare action defines 15 different channel functions that utilize capture, compare, and zero events. 0h = Disable channel. 1h = Set on capture, and then disable channel. Channel function sequence: - Set enabled events on capture event and copy CNTR.VALUE to CH1CC.VALUE. - Disable channel. Primary use scenario is to select this function before you start the timer. Follow these steps if you need to select this function while CTL.MODE is different from DIS: - Set CCACT to SET_ON_CAPT with no event enable. - Configure CH1CCFG (optional). - Wait for three timer clock periods as defined in PRECFG before you set CCACT to SET_ON_CAPT_DIS. Event enable is optional. These steps prevent capture events caused by expired signal values in edge-detection circuit. 2h = Clear on zero, toggle on compare, and then disable channel. Channel function sequence: - Clear enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH1CC.VALUE = CNTR.VALUE. - Disable channel. Enabled events are set when CH1CC.VALUE = 0 and CNTR.VALUE = 0. 3h = Set on zero, toggle on compare, and then disable channel. Channel function sequence: - Set enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH1CC.VALUE = CNTR.VALUE. - Disable channel. Enabled events are cleared when CH1CC.VALUE = 0 and CNTR.VALUE = 0. 4h = Clear on compare, and then disable channel. Channel function sequence: - Clear enabled events when CH1CC.VALUE = CNTR.VALUE. - Disable channel. 5h = Set on compare, and then disable channel. Channel function sequence: - Set enabled events when CH1CC.VALUE = CNTR.VALUE. - Disable channel. 6h = Toggle on compare, and then disable channel. Channel function sequence: - Toggle enabled events when CH1CC.VALUE = CNTR.VALUE. - Disable channel. 7h = Pulse on compare, and then disable channel. Channel function sequence: - Pulse enabled events when CH1CC.VALUE = CNTR.VALUE. - Disable channel. The event is high for two timer clock periods. 8h = Period and pulse width measurement. Continuously capture period and pulse width of the signal selected by CH1CCFG.CAPT_SRC relative to the signal edge given by CH1CCFG.EDGE. Set enabled events when CH1CC.VALUE contains signal period and CH1PCC.VALUE contains signal pulse width. Notes: - Make sure that you configure CH1CCFG.CAPT_SRC and CCACT when CTL.MODE equals DIS, then set CTL.MODE to UP_ONCE or UP_PER. - The counter restarts in the selected timer mode when CH1CC.VALUE contains the signal period. - If more than one channel uses this function, the channels will perform this function one at a time. The channel with lowest number has priority and performs the function first. Next measurement starts when current measurement completes successfully or times out. A timeout occurs when counter equals target. - If you want to observe a timeout event configure another channel to SET_ON_CAPT. Signal property requirements: - Signal Period >= 2 * ( 1 + PRECFG.CLKDIV ) * timer clock period. - Signal Period <= 65535 * (1 + PRECFG.CLKDIV ) * timer clock period. - Signal low and high phase >= (1 + PRECFG.CLKDIV ) * timer clock period. 9h = Set on capture repeatedly. Channel function sequence: - Set enabled events on capture event and copy CNTR.VALUE to CH1CC.VALUE. Primary use scenario is to select this function before you start the timer. Follow these steps if you need to select this function while CTL.MODE is different from DIS: - Select this function with no event enable. - Configure CH1CCFG (optional). - Wait for three timer clock periods as defined in PRECFG before you enable events. These steps prevent capture events caused by expired signal values in edge-detection circuit. Ah = Clear on zero, toggle on compare repeatedly. Channel function sequence: - Clear enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH1CC.VALUE = CNTR.VALUE. Set CTL.MODE to UPDWN_PER for center-aligned PWM generation. Duty cycle is given by: When CH1CC.VALUE <= TARGET.VALUE: Duty cycle = 1 - ( CH1CC.VALUE / TARGET.VALUE ). When CH1CC.VALUE > TARGET.VALUE: Duty cycle = 0. Enabled events are set when CH1CC.VALUE = 0 and CNTR.VALUE = 0. Bh = Set on zero, toggle on compare repeatedly. Channel function sequence: - Set enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH1CC.VALUE = CNTR.VALUE. Set CTL.MODE to UP_PER for edge-aligned PWM generation. Duty cycle is given by: When CH1CC.VALUE <= TARGET.VALUE: Duty cycle = CH1CC.VALUE / ( TARGET.VALUE + 1 ). When CH1CC.VALUE > TARGET.VALUE: Duty cycle = 1. Enabled events are cleared when CH1CC.VALUE = 0 and CNTR.VALUE = 0. Ch = Clear on compare repeatedly. Channel function sequence: - Clear enabled events when CH1CC.VALUE = CNTR.VALUE. Dh = Set on compare repeatedly. Channel function sequence: - Set enabled events when CH1CC.VALUE = CNTR.VALUE. Eh = Toggle on compare repeatedly. Channel function sequence: - Toggle enabled events when CH1CC.VALUE = CNTR.VALUE. Fh = Pulse on compare repeatedly. Channel function sequence: - Pulse enabled events when CH1CC.VALUE = CNTR.VALUE. The event is high for two timer clock periods. |
CH1CCFG is shown in Table 20-149.
Return to the Summary Table.
Channel 1 Capture Configuration
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-7 | RESERVED | R | 0h | Reserved |
| 6-1 | CAPT_SRC | R/W | 0h | Select capture signal source from the asynchronous AUX event bus. The selected signal enters the edge-detection circuit. False capture events can occur when: - the edge-detection circuit contains expired signal samples and the circuit is enabled without flush as described in CH1EVCFG - this register is reconfigured while CTL.MODE is different from DIS. You can avoid false capture events. When wanted channel function is: - SET_ON_CAPT_DIS, see description for SET_ON_CAPT_DIS in CH1EVCFG.CCACT. - SET_ON_CAPT, see description for SET_ON_CAPT in CH1EVCFG.CCACT. - PER_PULSE_WIDTH_MEAS, see description for PER_PULSE_WIDTH_MEAS in CH1EVCFG.CCACT. If you write a non-enumerated value the behavior is identical to NO_EVENT. The written value is returned when read. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
| 0 | EDGE | R/W | 0h | Edge configuration. Channel captures counter value at selected edge on signal source selected by CAPT_SRC. See CH1EVCFG.CCACT. 0h = Capture CNTR.VALUE at falling edge of CAPT_SRC. 1h = Capture CNTR.VALUE at rising edge of CAPT_SRC. |
CH1PCC is shown in Table 20-150.
Return to the Summary Table.
Channel 1 Pipeline Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Pipeline Capture Compare value. 16-bit user defined pipeline compare value or channel-updated capture value. Compare mode: An update of VALUE will be transferred to CH1CC.VALUE when the next CNTR.VALUE is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When CH1EVCFG.CCACT equals PER_PULSE_WIDTH_MEAS then VALUE contains the width of the low or high phase of the selected signal. This is specified by CH1CCFG.EDGE and CH1CCFG.CAPT_SRC. |
CH1CC is shown in Table 20-151.
Return to the Summary Table.
Channel 1 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Capture Compare value. 16-bit user defined compare value or channel-updated capture value. Compare mode: VALUE is compared against CNTR.VALUE and an event is generated as specified by CH1EVCFG.CCACT when these are equal. Capture mode: The current counter value is stored in VALUE when a capture event occurs. CH1EVCFG.CCACT determines if VALUE is a signal period or a regular capture value. |
CH2EVCFG is shown in Table 20-152.
Return to the Summary Table.
Channel 2 Event Configuration
This register configures channel function and enables event outputs.
Each channel has an edge-detection circuit with memory. The circuit is:
- enabled while CCACT selects a capture function and CTL.MODE is different from DIS.
- flushed while CCACT selects a capture function and you change CTL.MODE from DIS to another mode.
The flush action uses two AUX_SYSIF:TIMER2CLKCTL.SRC clock periods. It prevents capture events caused by expired signal values stored in the edge-detection circuit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | EV3_GEN | R/W | 0h | Event 3 enable. 0: Channel 2 does not control event 3. 1: Channel 2 controls event 3. When 0 < CCACT < 8, EV3_GEN becomes zero after a capture or compare event. |
| 6 | EV2_GEN | R/W | 0h | Event 2 enable. 0: Channel 2 does not control event 2. 1: Channel 2 controls event 2. When 0 < CCACT < 8, EV2_GEN becomes zero after a capture or compare event. |
| 5 | EV1_GEN | R/W | 0h | Event 1 enable. 0: Channel 2 does not control event 1. 1: Channel 2 controls event 1. When 0 < CCACT < 8, EV1_GEN becomes zero after a capture or compare event. |
| 4 | EV0_GEN | R/W | 0h | Event 0 enable. 0: Channel 2 does not control event 0. 1: Channel 2 controls event 0. When 0 < CCACT < 8, EV0_GEN becomes zero after a capture or compare event. |
| 3-0 | CCACT | R/W | 0h | Capture-Compare action. Capture-Compare action defines 15 different channel functions that utilize capture, compare, and zero events. 0h = Disable channel. 1h = Set on capture, and then disable channel. Channel function sequence: - Set enabled events on capture event and copy CNTR.VALUE to CH2CC.VALUE. - Disable channel. Primary use scenario is to select this function before you start the timer. Follow these steps if you need to select this function while CTL.MODE is different from DIS: - Set to SET_ON_CAPT with no event enable. - Configure CH2CCFG (optional). - Wait for three timer clock periods as defined in PRECFG before you set to SET_ON_CAPT_DIS. Event enable is optional. These steps prevent capture events caused by expired signal values in edge-detection circuit. 2h = Clear on zero, toggle on compare, and then disable channel. Channel function sequence: - Clear enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH2CC.VALUE = CNTR.VALUE. - Disable channel. Enabled events are set when CH2CC.VALUE = 0 and CNTR.VALUE = 0. 3h = Set on zero, toggle on compare, and then disable channel. Channel function sequence: - Set enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH2CC.VALUE = CNTR.VALUE. - Disable channel. Enabled events are cleared when CH2CC.VALUE = 0 and CNTR.VALUE = 0. 4h = Clear on compare, and then disable channel. Channel function sequence: - Clear enabled events when CH2CC.VALUE = CNTR.VALUE. - Disable channel. 5h = Set on compare, and then disable channel. Channel function sequence: - Set enabled events when CH2CC.VALUE = CNTR.VALUE. - Disable channel. 6h = Toggle on compare, and then disable channel. Channel function sequence: - Toggle enabled events when CH2CC.VALUE = CNTR.VALUE. - Disable channel. 7h = Pulse on compare, and then disable channel. Channel function sequence: - Pulse enabled events when CH2CC.VALUE = CNTR.VALUE. - Disable channel. The event is high for two timer clock periods. 8h = Period and pulse width measurement. Continuously capture period and pulse width of the signal selected by CH2CCFG.CAPT_SRC relative to the signal edge given by CH2CCFG.EDGE. Set enabled events when CH2CC.VALUE contains signal period and CH2PCC.VALUE contains signal pulse width. Notes: - Make sure that you configure CH2CCFG.CAPT_SRC and CCACT when CTL.MODE equals DIS, then set CTL.MODE to UP_ONCE or UP_PER. - The counter restarts in the selected timer mode when CH2CC.VALUE contains the signal period. - If more than one channel uses this function, the channels will perform this function one at a time. The channel with lowest number has priority and performs the function first. Next measurement starts when current measurement completes successfully or times out. A timeout occurs when counter equals target. - If you want to observe a timeout event configure another channel to SET_ON_CAPT. Signal property requirements: - Signal Period >= 2 * ( 1 + PRECFG.CLKDIV ) * timer clock period. - Signal Period <= 65535 * (1 + PRECFG.CLKDIV ) * timer clock period. - Signal low and high phase >= (1 + PRECFG.CLKDIV ) * timer clock period. 9h = Set on capture repeatedly. Channel function sequence: - Set enabled events on capture event and copy CNTR.VALUE to CH2CC.VALUE. Primary use scenario is to select this function before you start the timer. Follow these steps if you need to select this function while CTL.MODE is different from DIS: - Select this function with no event enable. - Configure CH2CCFG (optional). - Wait for three timer clock periods as defined in PRECFG before you enable events. These steps prevent capture events caused by expired signal values in edge-detection circuit. Ah = Clear on zero, toggle on compare repeatedly. Channel function sequence: - Clear enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH2CC.VALUE = CNTR.VALUE. Set CTL.MODE to UPDWN_PER for center-aligned PWM generation. Duty cycle is given by: When CH2CC.VALUE <= TARGET.VALUE: Duty cycle = 1 - ( CH2CC.VALUE / TARGET.VALUE ). When CH2CC.VALUE > TARGET.VALUE: Duty cycle = 0. Enabled events are set when CH2CC.VALUE = 0 and CNTR.VALUE = 0. Bh = Set on zero, toggle on compare repeatedly. Channel function sequence: - Set enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH2CC.VALUE = CNTR.VALUE. Set CTL.MODE to UP_PER for edge-aligned PWM generation. Duty cycle is given by: When CH2CC.VALUE <= TARGET.VALUE: Duty cycle = CH2CC.VALUE / ( TARGET.VALUE + 1 ). When CH2CC.VALUE > TARGET.VALUE: Duty cycle = 1. Enabled events are cleared when CH2CC.VALUE = 0 and CNTR.VALUE = 0. Ch = Clear on compare repeatedly. Channel function sequence: - Clear enabled events when CH2CC.VALUE = CNTR.VALUE. Dh = Set on compare repeatedly. Channel function sequence: - Set enabled events when CH2CC.VALUE = CNTR.VALUE. Eh = Toggle on compare repeatedly. Channel function sequence: - Toggle enabled events when CH2CC.VALUE = CNTR.VALUE. Fh = Pulse on compare repeatedly. Channel function sequence: - Pulse enabled events when CH2CC.VALUE = CNTR.VALUE. The event is high for two timer clock periods. |
CH2CCFG is shown in Table 20-153.
Return to the Summary Table.
Channel 2 Capture Configuration
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-7 | RESERVED | R | 0h | Reserved |
| 6-1 | CAPT_SRC | R/W | 0h | Select capture signal source from the asynchronous AUX event bus. The selected signal enters the edge-detection circuit. False capture events can occur when: - the edge-detection circuit contains expired signal samples and the circuit is enabled without flush as described in CH2EVCFG - this register is reconfigured while CTL.MODE is different from DIS. You can avoid false capture events. When wanted channel function is: - SET_ON_CAPT_DIS, see description for SET_ON_CAPT_DIS in CH2EVCFG.CCACT. - SET_ON_CAPT, see description for SET_ON_CAPT in CH2EVCFG.CCACT. - PER_PULSE_WIDTH_MEAS, see description for PER_PULSE_WIDTH_MEAS in CH2EVCFG.CCACT. If you write a non-enumerated value the behavior is identical to NO_EVENT. The written value is returned when read. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
| 0 | EDGE | R/W | 0h | Edge configuration. Channel captures counter value at selected edge on signal source selected by CAPT_SRC. See CH2EVCFG.CCACT. 0h = Capture CNTR.VALUE at falling edge of CAPT_SRC. 1h = Capture CNTR.VALUE at rising edge of CAPT_SRC. |
CH2PCC is shown in Table 20-154.
Return to the Summary Table.
Channel 2 Pipeline Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Pipeline Capture Compare value. 16-bit user defined pipeline compare value or channel-updated capture value. Compare mode: An update of VALUE will be transferred to CH2CC.VALUE when the next CNTR.VALUE is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When CH2EVCFG.CCACT equals PER_PULSE_WIDTH_MEAS then VALUE contains the width of the low or high phase of the selected signal. This is specified by CH2CCFG.EDGE and CH2CCFG.CAPT_SRC. |
CH2CC is shown in Table 20-155.
Return to the Summary Table.
Channel 2 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Capture Compare value. 16-bit user defined compare value or channel-updated capture value. Compare mode: VALUE is compared against CNTR.VALUE and an event is generated as specified by CH2EVCFG.CCACT when these are equal. Capture mode: The current counter value is stored in VALUE when a capture event occurs. CH2EVCFG.CCACT determines if VALUE is a signal period or a regular capture value. |
CH3EVCFG is shown in Table 20-156.
Return to the Summary Table.
Channel 3 Event Configuration
This register configures channel function and enables event outputs.
Each channel has an edge-detection circuit with memory. The circuit is:
- enabled while CCACT selects a capture function and CTL.MODE is different from DIS.
- flushed while CCACT selects a capture function and you change CTL.MODE from DIS to another mode.
The flush action uses two AUX_SYSIF:TIMER2CLKCTL.SRC clock periods. It prevents capture events caused by expired signal values stored in the edge-detection circuit.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | EV3_GEN | R/W | 0h | Event 3 enable. 0: Channel 3 does not control event 3. 1: Channel 3 controls event 3. When 0 < CCACT < 8, EV3_GEN becomes zero after a capture or compare event. |
| 6 | EV2_GEN | R/W | 0h | Event 2 enable. 0: Channel 3 does not control event 2. 1: Channel 3 controls event 2. When 0 < CCACT < 8, EV2_GEN becomes zero after a capture or compare event. |
| 5 | EV1_GEN | R/W | 0h | Event 1 enable. 0: Channel 3 does not control event 1. 1: Channel 3 controls event 1. When 0 < CCACT < 8, EV1_GEN becomes zero after a capture or compare event. |
| 4 | EV0_GEN | R/W | 0h | Event 0 enable. 0: Channel 3 does not control event 0. 1: Channel 3 controls event 0. When 0 < CCACT < 8, EV0_GEN becomes zero after a capture or compare event. |
| 3-0 | CCACT | R/W | 0h | Capture-Compare action. Capture-Compare action defines 15 different channel functions that utilize capture, compare, and zero events. 0h = Disable channel. 1h = Set on capture, and then disable channel. Channel function sequence: - Set enabled events on capture event and copy CNTR.VALUE to CH3CC.VALUE. - Disable channel. Primary use scenario is to select this function before you start the timer. Follow these steps if you need to select this function while CTL.MODE is different from DIS: - Set CCACT to SET_ON_CAPT with no event enable. - Configure CH3CCFG (optional). - Wait for three timer clock periods as defined in PRECFG before you set CCACT to SET_ON_CAPT_DIS. Event enable is optional. These steps prevent capture events caused by expired signal values in edge-detection circuit. 2h = Clear on zero, toggle on compare, and then disable channel. Channel function sequence: - Clear enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH3CC.VALUE = CNTR.VALUE. - Disable channel. Enabled events are set when CH3CC.VALUE = 0 and CNTR.VALUE = 0. 3h = Set on zero, toggle on compare, and then disable channel. Channel function sequence: - Set enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH3CC.VALUE = CNTR.VALUE. - Disable channel. Enabled events are cleared when CH3CC.VALUE = 0 and CNTR.VALUE = 0. 4h = Clear on compare, and then disable channel. Channel function sequence: - Clear enabled events when CH3CC.VALUE = CNTR.VALUE. - Disable channel. 5h = Set on compare, and then disable channel. Channel function sequence: - Set enabled events when CH3CC.VALUE = CNTR.VALUE. - Disable channel. 6h = Toggle on compare, and then disable channel. Channel function sequence: - Toggle enabled events when CH3CC.VALUE = CNTR.VALUE. - Disable channel. 7h = Pulse on compare, and then disable channel. Channel function sequence: - Pulse enabled events when CH3CC.VALUE = CNTR.VALUE. - Disable channel. The event is high for two timer clock periods. 8h = Period and pulse width measurement. Continuously capture period and pulse width of the signal selected by CH3CCFG.CAPT_SRC relative to the signal edge given by CH3CCFG.EDGE. Set enabled events when CH3CC.VALUE contains signal period and CH3PCC.VALUE contains signal pulse width. Notes: - Make sure that you configure CH3CCFG.CAPT_SRC and CCACT when CTL.MODE equals DIS, then set CTL.MODE to UP_ONCE or UP_PER. - The counter restarts in the selected timer mode when CH3CC.VALUE contains the signal period. - If more than one channel uses this function, the channels will perform this function one at a time. The channel with lowest number has priority and performs the function first. Next measurement starts when current measurement completes successfully or times out. A timeout occurs when counter equals target. - If you want to observe a timeout event configure another channel to SET_ON_CAPT. Signal property requirements: - Signal Period >= 2 * ( 1 + PRECFG.CLKDIV ) * timer clock period. - Signal Period <= 65535 * (1 + PRECFG.CLKDIV ) * timer clock period. - Signal low and high phase >= (1 + PRECFG.CLKDIV ) * timer clock period. 9h = Set on capture repeatedly. Channel function sequence: - Set enabled events on capture event and copy CNTR.VALUE to CH3CC.VALUE. Primary use scenario is to select this function before you start the timer. Follow these steps if you need to select this function while CTL.MODE is different from DIS: - Select this function with no event enable. - Configure CH3CCFG (optional). - Wait for three timer clock periods as defined in PRECFG before you enable events. These steps prevent capture events caused by expired signal values in edge-detection circuit. Ah = Clear on zero, toggle on compare repeatedly. Channel function sequence: - Clear enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH3CC.VALUE = CNTR.VALUE. Set CTL.MODE to UPDWN_PER for center-aligned PWM generation. Duty cycle is given by: When CH3CC.VALUE <= TARGET.VALUE: Duty cycle = 1 - ( CH3CC.VALUE / TARGET.VALUE ). When CH3CC.VALUE > TARGET.VALUE: Duty cycle = 0. Enabled events are set when CH3CC.VALUE = 0 and CNTR.VALUE = 0. Bh = Set on zero, toggle on compare repeatedly. Channel function sequence: - Set enabled events when CNTR.VALUE = 0. - Toggle enabled events when CH3CC.VALUE = CNTR.VALUE. Set CTL.MODE to UP_PER for edge-aligned PWM generation. Duty cycle is given by: When CH3CC.VALUE <= TARGET.VALUE: Duty cycle = CH3CC.VALUE / ( TARGET.VALUE + 1 ). When CH3CC.VALUE > TARGET.VALUE: Duty cycle = 1. Enabled events are cleared when CH3CC.VALUE = 0 and CNTR.VALUE = 0. Ch = Clear on compare repeatedly. Channel function sequence: - Clear enabled events when CH3CC.VALUE = CNTR.VALUE. Dh = Set on compare repeatedly. Channel function sequence: - Set enabled events when CH3CC.VALUE = CNTR.VALUE. Eh = Toggle on compare repeatedly. Channel function sequence: - Toggle enabled events when CH3CC.VALUE = CNTR.VALUE. Fh = Pulse on compare repeatedly. Channel function sequence: - Pulse enabled events when CH3CC.VALUE = CNTR.VALUE. The event is high for two timer clock periods. |
CH3CCFG is shown in Table 20-157.
Return to the Summary Table.
Channel 3 Capture Configuration
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-7 | RESERVED | R | 0h | Reserved |
| 6-1 | CAPT_SRC | R/W | 0h | Select capture signal source from the asynchronous AUX event bus. The selected signal enters the edge-detection circuit. False capture events can occur when: - the edge-detection circuit contains expired signal samples and the circuit is enabled without flush as described in CH3EVCFG - this register is reconfigured while CTL.MODE is different from DIS. You can avoid false capture events. When wanted channel function: - SET_ON_CAPT_DIS, see description for SET_ON_CAPT_DIS in CH3EVCFG.CCACT. - SET_ON_CAPT, see description for SET_ON_CAPT in CH3EVCFG.CCACT. - PER_PULSE_WIDTH_MEAS, see description for PER_PULSE_WIDTH_MEAS in CH3EVCFG.CCACT. If you write a non-enumerated value the behavior is identical to NO_EVENT. The written value is returned when read. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
| 0 | EDGE | R/W | 0h | Edge configuration. Channel captures counter value at selected edge on signal source selected by CAPT_SRC. See CH3EVCFG.CCACT. 0h = Capture CNTR.VALUE at falling edge of CAPT_SRC. 1h = Capture CNTR.VALUE at rising edge of CAPT_SRC. |
CH3PCC is shown in Table 20-158.
Return to the Summary Table.
Channel 3 Pipeline Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Pipeline Capture Compare value. 16-bit user defined pipeline compare value or channel-updated capture value. Compare mode: An update of VALUE will be transferred to CH3CC.VALUE when the next CNTR.VALUE is zero and CTL.MODE is different from DIS. This is useful for PWM generation and prevents jitter on the edges of the generated signal. Capture mode: When CH3EVCFG.CCACT equals PER_PULSE_WIDTH_MEAS then VALUE contains the width of the low or high phase of the selected signal. This is specified by CH3CCFG.EDGE and CH3CCFG.CAPT_SRC. |
CH3CC is shown in Table 20-159.
Return to the Summary Table.
Channel 3 Capture Compare
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | VALUE | R/W | 0h | Capture Compare value. 16-bit user defined compare value or channel-updated capture value. Compare mode: VALUE is compared against CNTR.VALUE and an event is generated as specified by CH3EVCFG.CCACT when these are equal. Capture mode: The current counter value is stored in VALUE when a capture event occurs. CH3EVCFG.CCACT determines if VALUE is a signal period or a regular capture value. |