SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Command ID number: 0x0601
CMD_READ_RFREG is an immediate command that takes the parameters listed in Table 26-41.
| Byte Index | Field Name | Bits | Bit Field Name | Type | Description |
|---|---|---|---|---|---|
| 0–1 | commandNo | W | The command ID number | ||
| 2–3 | address | W | The offset from the start of the RF core hardware register bank (0x4004 0000) | ||
| 4–7 | value | R | Returned value of the register |
On reception, the radio CPU reads the RF core register with address 0x40040000 + address. The result is written to value. If the address is not divisible by 4, the radio CPU returns ParError in RFC_DBELL:CMDSTA.
CMD_READ_RFREG may be sent as a direct command. If so, the address is given by bits 2–15 of CMDR, with the 2 LSBs of the address set to 00.
When reading is performed, the result is returned in value. The 24 LSBs of the result are returned in CMDSTA bits 8–31. The result returned in CMDSTA is Done.