SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Command ID number: 0x0405
CMD_ START_RAT is a direct command.
On reception, the radio CPU starts the RAT if it has not already started.
If the RAT is already running, the radio CPU returns the result ContextError in RFC_DBELL:CMDSTA. Otherwise, the radio CPU returns Done.