SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Source matching is performed on frames accepted by the frame filtering with a source address present. If the source address was an extended address, the received address is compared against the entries in the list pExtEntryList. If the source address was a short address, the received address and source pan ID are compared against the entries in the list pShortEntryList.
The number of entries that the lists can hold is given by numExtEntries and numShortEntries. If either of these values are 0, no source matching is performed on addresses of the corresponding type, and the corresponding pointer is NULL. The lists start with source mapping enable bits, srcMatchEn, and continue with pending enable bits, srcPendEn, followed by the list entries, see Table 26-74 and Table 26-75. The enable bits consist of the number of 32-bit words needed to hold an enable bit for each entry in the list. For each entry where the corresponding srcMatchEn bit is 1, the entry is compared against the received source address for extended addresses, or against the received source address and PAN ID for short addresses. If a match is found, the index is stored, and reported back in the message footer if configured (see Section 26.7.1). If no match is found, the index reported back is 0xFF.
The source matching procedure may also be used for finding the pending data bit to be transmitted in an auto-acknowledgment frame (see Section 26.5.4.1.3). If frameFiltOpt.autoPendEn is 1 and a source match was found, the pending data bit is set to the value of the bit in srcPendEn corresponding to the index of the match. If no match was found or if frameFiltOpt.autoPendEn is 0, the pending data bit is set equal to frameFiltOpt.defaultPend. If frameFiltOpt.bPendDataReqOnly is 1, the radio CPU investigates the frame to determine if it is a MAC command frame with the command frame identifier set to a Data Request. If not, the pending data bit of an auto ACK is set equal to 0, regardless of the source matching result and the value of frameFiltOpt.defaultPend.