SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
There are three subscribers in the AON event fabric as can be seen in Figure 5-2. The first subscriber is the MCU event fabric, which resides in the MCU power domain. The other two subscribers, the AON_PMCTL and RTC, both reside in the AON voltage domain and are presented in the following subsections.