SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
The procedure takes the following input parameter:
The procedure returns the following:
The procedure returns with error if the specified queue is empty, or if the first entry of the queue is already busy. Otherwise, the following is done:
set pQueue->pCurrEntry->status = Busy
set pEntry = pQueue->pCurrEntry