DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1 , DLPC231-Q1 , DLPC231S-Q1
This command tells the boot application to verify the contents of the flash device.
The Request in Progress bit of the Short Status will be set at the start of the flash verify process and will be cleared when the verify process is complete.
Once the process is completed, the error bits in the Short Status can be used to determine whether an error occurred during the verification process.
More information on flash programming can be found in Section 5.3.3.
Write Parameters
No write parameters.