DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1 , DLPC231-Q1 , DLPC231S-Q1
This command is used to set TPS99000-Q1 TIA1 RGB input offsets.
Write Parameters
| BYTE | BITS | DESCRIPTION |
|---|---|---|
| 1 | 2:0 | Red Input Offset Offset = (N+1) × 20mV 0x7 = 0mV. This value is an exclusion from the formula above and should not be used because the amplifier requires offset. |
| 2 | 2:0 | Green Input Offset Offset = (N+1) × 20mV 0x7 = 0mV. This value is an exclusion from the formula above and should not be used because the amplifier requires offset. |
| 3 | 2:0 | Blue Input Offset Offset = (N+1) × 20mV 0x7 = 0mV. This value is an exclusion from the formula above and should not be used because the amplifier requires offset. |
| 4 | 2:0 | Default Input Offset This default is used when no illumination enable is active during the sequence time. Offset = (N+1) × 20mV 0x7 = 0mV. This value is an exclusion from the formula above and should not be used because the amplifier requires offset. |