DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1 , DLPC231-Q1 , DLPC231S-Q1
This command is used to read back the host-specified values for the loss-of-dimming-command function.
Command Parameters
No command parameters.
Return Parameters
| BYTE | BITS | DESCRIPTION |
|---|---|---|
| 1 | 7:0 | Timeout length Maximum allowed time in milliseconds between dimming command transmissions. 0 = Disable |