DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1 , DLPC231-Q1 , DLPC231S-Q1
This command is used to enable the loss-of-dimming-command test and to specify the maximum allowable time between dimming commands. The default value for this function is specified in flash data.
Section 6.4.1.5 describes the loss-of-dimming test in more detail.
Write Parameters
| BYTE | BITS | DESCRIPTION |
|---|---|---|
| 1 | 7:0 | Timeout length Maximum allowed time in milliseconds between dimming command transmissions. 0 = Disable For example, 16 = host must continuously send a command within 16-ms time frame. |