DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1 , DLPC231-Q1 , DLPC231S-Q1
HOST_SPI_MODE is configured as an output and toggled during DLPC230-Q1 software initialization to aid in debug. This begins immediately after the value is read as an input. Figure 2-2 shows the initialization events and the associated HOST_SPI_MODE signal. A toggle will occur for optional events regardless of whether they are enabled or disabled so that events following can still be properly identified.
Figure 2-2 Boot Flow DebugThe tests are described in Section 6.4.2. BIST 1 is the DLPC230-Q1 Command and Flash Interface Memory Test.