SPRUIX0D February 2021 – August 2021
Four UART ports of the SoC are interfaced with FT4232H for UART-to-USB functionality and terminated on a micro B connector (J26). When the EVM is connected to a Host using the provided USB cable, the host can establish a Virtual Com Port which can be used with any terminal emulation application. The FT4232H is bus powered. Virtual Com Port drivers for the FT4232H can be obtained from https://www.ftdichip.com/Products/ICs/FT4232H.htm.
The FT_Prog has three modes of operation: Idle Mode, Program Mode and Edit Mode. FT_Prog programming parameters can be saved in files referred as EEPROM templates. Once defined, these EEPROM templates can be loaded by FT_Prog and used to program EEPROMs.
Figure 3-13 AM64x/AM243xUART Interfaces