SPRUIX0D February 2021 – August 2021
The DP83867 PHY uses four level configurations based on resistor strapping, which generates four distinct voltages ranges. The resistors are connected to the RX data and control pins that are normally driven by the PHY and are inputs to the AM64x. The voltage range for each mode is shown below:
Mode 1 - 0 V to 0.3234 V
Mode 2 – 0.462 V to 0.6303 V
Mode 3 – 0.7425 V to 0.9372 V
Mode 4 – 2.2902 V to 2.904 V
DP83867 device includes internal pull-down resistor. The value of the external pull resistors is selected to provide voltage at the pins of the AM64x/AM243x as close to ground or 3.3V as possible. The strapping is shown in Figure 3-21 and strap values shown in Table 3-19.
Address strapping is provided for CPSW PHY to set address -00000 (0h) by default, as strapping pins has internal pull-down resistors. Footprint for both pull up and pull down is provided on all the strapping pins except LED_0. LED_0 is for Mirror Enable, which is set to mode 1 by default, Mode 4 is not applicable and Mode2, Mode3 option is not desired.