SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
Seven output events from the AON event fabric are routed as inputs to the MCU event fabric. These events are:
There are three programmable lines from which any of the input events from Table 6-5 can be chosen. This can be set in the CTRL_EVENT:MCU register.