SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
Command ID number: 0x0010
CMD_SET_TX_POWER is an immediate command that takes the parameters listed in Table 26-48.
| Byte Index | Field Name | Bits | Bit Field Name | Type | Description |
|---|---|---|---|---|---|
| 0–1 | commandNo | W | The command ID number | ||
| 2–3 | txPower | W | New TX power setting. TI recommends using
values from the SmartRF Studio. Bits 0-6: IB Value to write to the PA power control field at 25°C. Check the note below. Bits 6-7: GC Value to write to the gain control of the first stage of the PA. Bit 8: boost Driver strength into the PA. 0: Low driver strength 1: High driver strength Bits 9-15: tempCoeff Temperature coefficient for IB. 0: No temperature compensation. |
On reception, the radio CPU sets the transmit power for use the next time transmission begins. If a packet is being transmitted, the transmit power is not updated until transmission begins for the next packet.
Each time transmission of a packet begins, temperature compensation of the transmit power is done.
It is not allowed to use CMD_SET_TX_POWER if the 20 dBm PA was configured in the radio setup command; in this case, CMD_SET_TX20_POWER (see Section 26.3.3.2.17) should be used.
On completion, the radio CPU returns DONE in CMDSTA.