SWCU193 April 2023 CC2340R2 , CC2340R5 , CC2340R5-Q1
The PMCTL subscriber has 6 programmable events in AON event fabric, which are ORed together to form a single wake-up event to PMCTL configurable via the EVTULL.WKUPMASK register. This wake-up event is used to trigger the wakeup of the MCU power domain from Standby mode. Any of the events listed in Table 4-4 can be chosen as input by selecting the appropriate event publisher or publishers. By default, this register is set to 0, meaning that no publishers are selected to drive the wake-up event towards PMCTL.