SWCU193 April 2023 CC2340R2 , CC2340R5 , CC2340R5-Q1
The DSSM provides 4 interrupt sources which can be configured to source a CPU interrupt event. The CPU interrupt events from the DSSM are given in Table 5-6.
Name | Description |
---|---|
TXIFG | Indicates that the TX_DATA buffer in the DSSM has received data. |
RXIFG | Indicates that the data in RX_DATA buffer in the DSSM was read. |
PWRUPIFG | Indicates that the DEBUGSS was started due to a debug probe attaching to the device. |
PWRDWNIFG | Indicates that the DEBUGSS was stopped due to a debug probe disconnecting from the device. |
See Chapter 62 for guidance on configuring the DEBUGGSS event as a CPU interrupt.