SWCU193 April 2023 CC2340R2 , CC2340R5 , CC2340R5-Q1
There are three subscribers in the AON event fabric as can be seen in Figure 4-3. The first subscriber is the MCU event fabric, which resides in the MCU power domain. The other two subscribers, the PMCTL and RTC, are presented in the following subsections.