This command sends the device into ROM mode in
preparation for firmware reprogramming. To enter ROM mode, the device must be in
FULL ACCESS mode.
Note: Executing
the traditional 0x08 command will not work. BQ41z device family erases the flash
memory once device enters ROM mode. User will have to re-program the flash sector
and execute the ROM command 0x88 0x09.