SLUUCP8B June 2024 – October 2026 BQ41Z50
The BQ41Z50 device can stop charging if it measures a difference between the requested ChargingVoltage() and the delivered voltage from the charger. This feature only operates when the device is in CHARGE mode.
ChargingVoltage() will be set to 0mV when the protection is tripped. The ChargingVoltage() for the recovery is the intended or targeted charging voltage, not the 0mV that was set due to the trip of protection.
| Status | Condition | Action |
|---|---|---|
| Normal | PACK voltage in DAStatus1() < ChargingVoltage() + CHGV:Threshold× Number of series cells | SafetyAlert()[CHGV] = 0 |
| Alert | PACK voltage in DAStatus1() ≥ ChargingVoltage() + CHGV:Threshold× Number of series cells | SafetyAlert()[CHGV] = 1 BatteryStatus()[TCA] = 1 |
| Trip | PACK voltage in DAStatus1() ≥ ChargingVoltage() + CHGV:Threshold× Number of series cells for CHGV:Delay period | SafetyAlert()[CHGV] = 0 SafetyStatus()[CHGV] = 1 BatteryStatus()[TCA] = 0 OperationStatus()[XCHG] = 1 |
| Recovery | SafetyStatus()[CHGV] = 1 AND PACK voltage in DAStatus1() ≤ intended ChargingVoltage() + CHGV Recovery× Number of series cells | SafetyStatus()[CHGV] = 0 BatteryStatus()[TCA] = 0 OperationStatus()[XCHG] = 0 |