SLUUCP8B June 2024 – October 2026 BQ41Z50
The following is the charging voltage degradation process:
When a Degradation Mode is entered, whether though cycle count based, SOH based, or runtime based degradation, the highest degradation mode determines the level of ChargingVoltage() adjustment.
In NORMAL mode, no ChargingVoltage() adjustment is applied.
Entering Degradation Mode 1, ChargingVoltage() is reduced by Voltage Degradation for Mode 1. Enterning Degradation Mode 2, ChargingVoltage() is reduced by Voltage Degradation for Mode 2. Similarly for entering Degradation Mode 3, as the ChargingVoltage() is reduced by Voltage Degradation for Mode 3. The charging voltage mode reduction is a one-way transition. The gauge only goes from Normal → Lvl1 → Lvl2 → Lvl3. The three degradation points each occur one time when the Degradation Mode is reached due to any of the cycle count, SOH, or runtime based degradation criteria.
This charging voltage degradation scheme (if enabled) works in conjunction with any other existing degradation/increments (such as charging loss compensation).