SPRAD21J May 2022 – October 2026 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1
The DC current outputs sourced by the processor IO configured as output needs to remain less than the maximum IOH and IOL values defined to achieve the VOL maximum and VOH minimum values defined in the Electrical Characteristics table. The output currents defined in the processor-specific datasheet shall not be used as limits for steady-state currents. The datasheet output current limits are only expected to be reached when charging or discharging signal capacitance to transition a signal from low to high or from high to low. Once the signal reaches a valid logic state, the steady-state current is expected to be much lower than the datasheet current limit values. The outputs can tolerate some level of steady-state current as required to over-drive typical pull resistors, but we do not expect large steady-state current like what is needed to drive an LED or similar load continuously. The recommendation is to use an external FET or transistor switch controlled by processor IO to drive LEDs or similar loads that can draw continuous current.