SPRAD21J May 2022 – October 2026 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1
The recommendation is to consider adding the required or applicable design notes for the processor, attached devices and other on-board devices to reduce errors during custom board design. The recommendation is to add the required design notes for the processor memory (Example: USB2.0 interface, Ethernet interface, Camera interface, Display interface ((OLDI0 (AM625, AM623, AM625-Q1, AM625SIP and AM62P, AM62P-Q1) and DSITX0 (AM62P, AM62P-Q1)) including eMMC, OSPI, SD card, SDIO and other used processor peripherals including USB, MCSPI, MCASP). The recommendation is to include notes to include custom board boot mode configurations, placement of series and parallel resistors, placement of decoupling and bulk capacitors.
The recommendation is to mark all differential signals, critical signals that can affect performance and specify the target impedance (as required). See the following examples:
Refer to the AM62Ax, AM62Px, AM62Dx LPDDR4 Board Design and Layout Guidelines for the recommended target impedance for the LPDDR4 clock, address and control signals.
See the following FAQs that includes board layout guideline to follow:
[FAQ] AM625: PCB Pattern Recommendations for Specific Peripherals
[FAQ] AM625: MMC0 PCB Connectivity Requirements
AM6442: PCB layout guidelines for MMCSD0(eMMC) and MMCSD1(SD card)
The FAQs are generic and can also be used for AM62x (AM625, AM623, AM620-Q1, AM625-Q1, AM625SIP), AM62Ax (AM62A7, AM62A7-Q1, AM62A3, AM62A3-Q1, AM62A1-Q1), AM62D-Q1 and AM62Px (AM62P, AM62P-Q1) processor families.
For more information, see the following FAQ: