SLOS893D September 2014 – August 2025 DRV2624
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
To capture the graphs displayed in the Typical Characteristics section, the following first-order RC-filter setup is used with the exception of the waveform in Figure 6-1 which is captured without any output filter. The filter is used when viewing output signals on an oscilloscope because output PWM modulation is present in all modes. Maintain that effective impedance of the filter is not too low because the closed-loop and auto resonance-tracking features can be affected. Therefore, TI recommends that this exact filter be used for output measurement. Most oscilloscopes have an input impedance of 1MΩ on each channel and therefore have an approximately 1% loss in measured amplitude because of the voltage-divider effect with the filter.
Figure 6-1 Test Setup