SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Starting with CLB Type 2, the Counter module operates as a linear feedback shift register. By configuring the characteristics of the LFSR, the counter module is used to compute the CRC on a serial bit stream. The polynomial for LFSR is in the MATCH2 reference register. The feedback bit position is in the MATCH1 reference register.
To enable the LFSR mode, CLB_MISC_CONTROL.COUNT_SERIALIZER_0 (for Counter 0) must be set along with COUNT0_LFSR_EN.
There are two types of LSFR that can be selected by changing the MODE1 value (0 or 1), as shown in Figure 29-13.