SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The CLB X-BAR brings signals to the CLB modules. Figure 10-3 shows the architecture of the CLB X-BAR. Note that the architecture of the CLB X-BAR is identical to the architecture of the GPIO Output X-BAR (with the exception of the output latch).