SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The ePIE vector table memory is protected using a parity check. Upon each vector fetch from the ePIE, a parity check is performed. If a parity failure occurs during vector fetch, the ePIE returns either a user defined error handler routine (if PIEVERRADDR is defined with a non 0x003FFFFF value), or the default boot ROM handler at address 0x3FFFBE. The ePIE also sends trip signals to the EPWMs.
The parity check only returns the error handler value if the failure occurs during vector fetch. Parity errors during data read is handled by the memory controller module and logged by UCERRFLG register in MEMORY_ERROR_REGS. The address that caused the error is located in the UCCPUREADDR register. If the error address logged is between 0xD00 to 0xDFF, then the error is a PIE parity error. Additionally, a parity error during vector fetch does not flag an uncorrectable error NMI.