SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The Enhanced Bus Comparator (EBC) units connect to the CPU using a direct memory interface. This includes the program address and data buses, the data address, write and read data buses, debug qualifiers for memory access, and the ability to set breakpoints, watch points, and trace points on the CPU. Typically, the EBC is owned and controlled by the debugger application (for example, Code Composer Studio™ IDE). A user application running on the CPU can also configure and use the EBC units to generate events and interrupts for real-time diagnostic purposes. Note that ownership is exclusive—the debugger and application software cannot simultaneously control an EBC unit. For more information on EBC unit ownership, see Section 12.4.
The EBC units have the following capabilities:
The following features are not supported by the EBC units:
Each EBC unit has the capability to monitor a range of addresses by defining masks and generating outputs based on greater than, less than, or equal events.
The EBC units can also be used with the System Event Counter (SEC) units for system or code profiling and analysis purposes.