SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Flash memory can be programmed either by using the CCS Flash plug-in or by using the UniFlash application. If these methods are not feasible in an application, the Flash API can be used. The Flash memory can be programmed, erased, and verified only by using the Flash API library. These functions are written, compiled and validated by Texas Instruments. The Flash module contains a Flash state machine (FSM) to perform program and erase operations.
The recommended flow for programming
Flash is:
Erase → Program → Verify