SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
If local shared RAM is configured as dedicated RAM for the CPU, or if it is configured as program RAM for the CLA, any data write access from the CLA to that particular LSx RAM results in a CLA write protection violation, which is a non-controller access violation.
If a CLA write protection violation occurs, the write gets ignored, a flag gets set in the appropriate access violation flag register, and the memory address for which the access violation occurred, gets latched in the appropriate CLA write access violation address register. Also, an access violation interrupt is generated to the CPU if enabled in the interrupt enable register.