SPRABY1B February   2015  – November 2026 F28M35E20B , F28M35H22C , F28M35H52C , F28M35H52C-Q1 , F28M35M22C , F28M35M52C , F28M36H33B2 , F28M36H53B2 , F28M36P53C2 , F28M36P63C2 , F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1 , SM320F2801-EP , TMS320C28341 , TMS320C28342 , TMS320C28343 , TMS320C28343-Q1 , TMS320C28344 , TMS320C28345 , TMS320C28346 , TMS320C28346-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F2801 , TMS320F2801-Q1 , TMS320F28015 , TMS320F28016 , TMS320F28016-Q1 , TMS320F2802 , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1 , TMS320F28044 , TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28053 , TMS320F28054 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F28055 , TMS320F2806 , TMS320F2806-Q1 , TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1 , TMS320F2808 , TMS320F2808-Q1 , TMS320F2809 , TMS320F2810 , TMS320F2810-Q1 , TMS320F2811 , TMS320F2811-Q1 , TMS320F2812 , TMS320F2812-Q1 , TMS320F28232 , TMS320F28232-Q1 , TMS320F28234 , TMS320F28234-Q1 , TMS320F28235 , TMS320F28235-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   MSL Ratings and Reflow Profiles
  3.   Trademarks
  4. 1Introduction
  5. 2Applying the Moisture Sensitivity Level (MSL)
  6. 3MSL Classification Peak Reflow Temperature
  7. 4MSL Classification Reflow Profile for Lead-Free Soldering
  8. 5Customer Board Assembly Reflow Profile for Lead Free Soldering
  9. 6Wave Soldering
  10. 7References
  11. 8Revision History

MSL Classification Reflow Profile for Lead-Free Soldering

The Classification Profile (Not to scale) table in the IPC/JEDEC-020 shows the classification reflow profile to be used for the device MSL classification/certification by the component manufacturer with the maximum reflow temperature Tp.

Table 3-1 lists temperatures is the Tc (Classification temperature). For the new product classification, the Tp is higher than the Tc.

 TI Representation of the J-STD-020 Classification Profile (not to scale)Figure 4-1 TI Representation of the J-STD-020 Classification Profile (not to scale)

Figure 4-1 illustrates the key temperature/times associated with the different Reflow oven zones. Important items defined in J-STD-020 that can impact IC reliability are:

  • Soak time ts
  • Soak temperatures: min(Tsmin) and max (Tsmax)

During the Preheat/Soak, the board and components are reaching a temperature where the flux in the solder paste is starting its activity and cleaning process of all surfaces involved into the later solder joint begins.

  • Liquidous temperature (TL) for lead-free soldering - this is approximately 217°C. This varies according to the used solder alloy.
  • The Peak temperature (Tp) for the reflow profile, measured at top of the package.
    • For the user (board assembly process), Tp must not exceed Tc as shown in Table 3-1. For the IC suppier, the Tp is ≥ Tc.
    • Time that defines the peak temperate (tp) starts/ends -5°C below Tp.
  • Ramp up rate from TL to TP (must not exceed 3°C/second)
  • Time from 25°C (room temperature) to peak temperature should not exceed 8 minutes.
  • Cool down rate from TP to TL (must not exceed -6°C/second)