SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The timer manager must be disabled (clear TIMERMGR_CNTL[0] ENABLE to 0) before the timer manager is powered down. The timer manager will only be idle if it is not enabled and the event FIFO is empty – an enabled Timer Manager means the state machine is running and the timer manager is waiting for expired timers.
To power up the Timer Manager if it has been powered down but not reset, the timer values in the timer RAM must be assumed to be invalid. Any timers must either be reprogrammed (TIMER_SET) before the timer is re-enabled. If this is not done, the Timer Manager may report timeouts as soon as it is enabled.
Additionally, all timers that have expired must be cleared before disabling the Timer Manager, otherwise there will be no Event Down generated on the event interface to clear the expired timers from the interrupt aggregator. This effectively means that software must disable all timers before writing a 0 to TIMERMGR_CNTL[0] ENABLE.
The event FIFO will continue to drive pending events even if the Timer Manager is disabled, so the remaining Event Down actions will still occur – software only needs to disable the timers to ensure that the Event Down commands are pushed into the event FIFO but does not need to wait for the event FIFO to flush before disabling the timer manager.