SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The error register bank handles storing all error flags that are identified. It also stores some status bits that must be observable and detectable by the application. These status and error registers can generate an interrupt on the rising or falling edge if this generation is enabled.
This mechanism is different depending on the nature of the status or error bits. For those that are generated in the DSI block (basically all status and error bits except direct command), the status bits cannot be easily controlled and toggle according to the internal status meaning only the current value is observed in the status/error register itself.
If the interrupt generation is enabled with the associated enable bit, a rising edge (associated edge bit set to 0) or a falling edge (associated edge bit set to 1) of that status bit toggles the corresponding flag bit. At the end, all the flag bits are put together with an OR to generate the interrupt signal. The flag register can be reset by writing in the clear register.
The described behavior can be summarized by the following pseudo-HDL. The signal named signal_sts_bit is the bit that is observable by reading status bit.
reg_sts_d <= signal_sts_bit;
reg_flag_sts_d <= '0' WHEN clear_the_flag = '1' ELSE
irq_n <= NOT (OR_OF_ALL(reg_flag_sts_q AND enable_sts_ctl));
The code is slightly different in cases where the observed bit is a generated condition (in the control block), as is the case for the direct command status and error flags. The status/error information is automatically generated but is cleared only when writing in the corresponding clear bit. The interrupt generation behaves similarly to the error condition cases, however, as the status falling edge is observed only when the bit is cleared, it is not possible to use the falling edge detection on flag (however the code is kept as-is to provide a standard implementation method). This leads to the following code:
Note: In some case (pulse generated), the rising edge detection is not done and the code becomes simply '1' WHEN signal_sts_bit = '1' ELSE...