SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
If a transaction times out and a Transaction Timeout Interrupt is asserted (and there are no currently outstanding Interrupts) then the following registers are loaded with the information about the transaction that timed out:
The Timeout Error Info Register (Base Address + 0x30) register keeps track of how many Transaction Timeout Interrupts have occurred since the last one was serviced. When a Transaction Timeout Interrupt occurs, the value is incremented (until saturated). If a Transaction Timeout Interrupt occurs and there is already one pending, then the counter is incremented by one, but the reporting information for the new transaction is lost.