SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
The AASRC channel is controlled primarily via the PDMA_PSILCFG_RX_AASRC_RX_FIFO_CONFIG register for the channel. This register holds three basic pieces of information:
The channel will remain idle until a pulse is detected on ALL associated input DMA request event pins required by the PDMA_PSILCFG_RX_AASRC_RX_FIFO_CONFIG setting. The pulses for the individual events are latched and held by the PDMA until they all arrive. Once the channel activates, it will start reading FIFO index values from RX order table (PDMA_PSILCFG_RX_AASRC_RX_ORDER_TABLE0, PDMA_PSILCFG_RX_AASRC_RX_ORDER_TABLE1), starting at the configured FIRSTSLOT and ending with the LASTSLOT. The actual FIFO indices used are obtained from the ordering table. For example, say FIRSTSLOT=3 and LASTSLOT=5. If the first 6 slots of the ordering table were: 0, 2, 4, 6, 8, 10, the FIFOs read for the event would be 6, 8, and 10, because 'slot 3' of the table contains 6, and it would proceed through 'slot 5' of the table which contains 10.
The X and Y registers are still used as they are in a normal X-Y mode. When accessing each FIFO, the setting of X determines the sample byte width read from the FIFO. The value of 'Y' determines how many times the entire FIFO list is processed for each activation of the channel. Once the total specified number of transactions has been completed the channel will return to an idle state and wait until it is triggered again. The read transfers that are performed will be accomplished as quickly as possible given availability of data in the TX channelized FIFO and given the arbitration that may occur as a result of other channels also using the same write unit.