SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
If two or more controller transmitters start a transmission on the same bus almost simultaneously, an arbitration procedure is invoked. The arbitration procedure uses the data presented on the serial bus by the competing transmitters. When a transmitter senses that a high signal it has presented on the bus has been overruled by a low signal, it switches to the target receiver mode, sets the arbitration lost (I2C_IRQSTATUS_RAW[0] AL) flag, and generates the arbitration lost interrupt. Figure 12-122 shows the arbitration procedure between two devices. The arbitration procedure gives priority to the device that transmits the serial data stream with the lowest binary value. If two or more devices send identical first bytes, arbitration continues on the subsequent bytes.
Figure 12-122 I2C Arbitration Between
Controller Transmitters