SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
The Info Register contains information about the current status of the gasket.
| Bits | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31:25 | Reserved | r | 0x0 | Reserved. Read as 0. |
| 24:16 | cur_writes | r | 0x0 | This is the current number of occupied slots in the write scoreboard. |
| 15:9 | Reserved | r | 0x0 | Reserved. Read as 0. |
| 8:0 | cur_reads | r | 0x0 | This is the current number of occupied slots in the read scoreboard |