SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
Ethernet port N (where N = 1 to 4)
The total number of frames received on the port that experienced an alignment error or code error. Such a frame:
Overruns have no effect upon this statistic.
An alignment error is defined to be:
A code error is defined to be a frame which has been discarded because the port’s MRXER pin driven with a one for at least one bit-time’s duration at any point during the frame’s reception.
RFC 1757 etherStatsCRCAlignErrors Ref. 1.5 can be calculated by summing Rx Align/Code Errors and Rx CRC errors.