JAJSRK3A December 2021 – November 2023 BQ79631-Q1
PRODUCTION DATA
Transaction frames are created using the frame structure discussed in the previous sections. This section outlines how the command and response frames are passing through the daisy-chain. The CRC values in the examples are correct and can be used to verify the customer CRC algorithm. The CRC is verified by the device with every received command frame and the command is not executed unless the CRC is valid.