SPRADO3B December 2024 – September 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
If the custom board uses USB Micro-AB connector, the USBn_ID signal from the connector is recommended to be routed to any of the processor pin. The GPIO pin used can be specified in the board device tree file, including the pinmux setting of the GPIO pin.