General
Review and verify the following for the custom
schematic design:
- Reviewed above "Common checklist for all
sections" section of the user's guide.
- Implementation approach of VPP supply and
isolation of supply.
- Recommended operating conditions for OTP eFuse
programming.
- Control of VPP supply (LDO EN).
- Recommended bulk and filter capacitors.
- Connection recommendations for external
supply.
- External VPP supply timing control.
- VPP supply sequence.
- Connecting the VPP supply to a continuous 1.8V
supply rail is not recommended or allowed or
supported option.
Schematic Review
Follow the list below for the custom schematic
design:
- Recommended bulk and filter capacitors are
provided (follow SK schematic
implementation).
- Processor supply rail connected to the VPP
supply (for eFuse programming) follows the
processor ROC.
- Implementation of on-board supply or provision
to connect external supply with the bulk and
decoupling capacitors added on the processor
board.
- A fixed output LDO or PMIC output (maximum
current of 400mA) is recommended (use of FET based
switch or Load switch is not recommended or
allowed).
- Choose on-board LDO that with nominal voltage
of 1.8V and supports a minimum current of 400mA,
has good load current transient response, and
quick output discharge (active discharge)
capability. Follow the LDO specs used on the SK
schematics.
- When an adjustable LDO is used, the
recommendation is to verify the output voltage
configuration, output voltage accuracy, output
voltage slew and use of output over voltage
protection (zener).
- Processor IO is used to control the EN of the
LDO and the recommended pull is provided.
- The recommendation is to verify if EN pull
holds the LDO in off-state during and after power
cycling.
- When external supply is connected, the
recommendation is to add bulk and decoupling
capacitor provision on the processor board near to
the processor VPP pin and provided a TP to connect
the external supply.
- External VPP supply (when used) follows the
recommended power sequence and slew rate
requirements as per the processor-specific data
sheet.
Additional
- The recommendation is to always
provide provision on the processor board to connect VPP supply (on-board or
external supply).
- The recommendation is to connect
LDO output to the processor VPP pin with a low loop inductance path to source
the high load current transients, where the supply on the VPP pin never drops
below the minimum operating voltage.
- Series resistor or jumper is provided to isolate the processor VPP supply from
the LDO output for testing the timing or LDO output. The resistor package is
expected to be rated for current > 400mA.
- When an adjustable output LDO is used,
consider adding an external zener based over
voltage protection at the LDO output and provide
provision to isolate the LDO output connected VPP
supply pin to test the LDO output.
- Due to the load current transient requirement
during eFuse programming, using load switch or FET
based switch is not recommended. A load switch or
FET based switch is likely to have higher voltage
drop that is not compensated.
- If the use case requires use of load switch or
FET based switch, the recommendation is to
characterize the board performance by measuring
the voltage on the processor VPP pin during
programming and verify that VPP supply never drops
below the ROC minimum value. Several variables in
the path of VPP supply can cause the supply to be
out of the ROC and are required to be
characterized before implementing. Check if the
load switch or FET based switch violates the
maximum VPP supply slew rate requirement defined
in the processor-specific data sheet.
- The recommendation is to leave the processor
VPP supply pin floating (Hi-Z) or grounded during
power-up sequences, power-down sequences, and
normal device operation.