SPRADO3B December 2024 – September 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
During the custom board design cycle, the recommendation is to follow Hardware Design Considerations for Custom Board Design Using AM625, AM623, AM620-Q1, AM625-Q1, AM625SIP Processor Family user's guide along with Schematic Design Guidelines and Schematic Review Checklist user's guide.
The next phase of the custom board design once the required schematics updates are complete (following the user's guide, referring to the SK schematic implementation, hardware design considerations user's guide and other collaterals on TI.com), is to perform a self-review following the review checklist provided at the end of each section of the schematic design guidelines. Schematic review checklist in excel format can be used alternatively to perform the review and the schematics in excel format can be used to track the completion of schematic review section wise.
Example of schematic review checklist sections for self-review:
The below FAQ lists the available collaterals and review steps that can be followed by custom board designer while performing a self-review of custom board schematics:
The below FAQ lists common errors observed (based on review of multiple customer schematics and reference to multiple collaterals). The recommendation is to read the list of errors and make the required updates to the custom board schematics: