General
Review and verify the following for the custom
schematic design:
- Reviewed above "Common checklist for all
sections" section of the user's guide.
- Connection (termination) of PORz_OUT, RESETSTATz and MCU_RESETSTATz status
outputs.
- Reviewed MCU_RESETSTATz related silicon errata.
- IO level compatibility between the processor reset status output and
attached device reset input.
- Capacitor load connection at the output of reset status output.
- Reset status output when not used.
- External ESD protection for the reset status outputs when connected to
carrier board or external connector.
Schematic Review
Follow the below list for the custom
schematic design:
- PORz_OUT is used as input to latch the processor boot mode configuration or
attached device strap configuration during processor cold reset.
- RESETSTATz, MCU_RESETSTATz is used to reset the attached devices when the
processor undergoes any type of global reset (cold or warm).
- PORz_OUT, MCU_RESETSTATz and RESETSTATz have pulldown added to hold the attached
devices in reset during supply ramp and processor reset near to the processor
pin.
- Connection of capacitor directly on the reset output near to the reset input of
the attached device (capacitor > 22pF). Perform simulation.
- IO level compatibility between the processor reset status output and attached
device reset input (can cause residual voltage affecting custom board
performance).
- Provision for TP provided when any of the reset status outputs are not
used.
- Processor reset output IO level and the attached device input IO levels are
recommended to be matched to avoid voltage leakage.