SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
MAC Port 1: link up prints but Board IP never appears. The application waits indefinitely for DHCP.
| Cause | How to Check | Fix |
|---|---|---|
| No DHCP server on the network | The PC has no DHCP server running. The board sends DISCOVER with no response. | Run dnsmasq on the PC, or switch to static IP: set #define USE_DHCP 0 in lwipcfg.h:73. |
| The broadcast ALE entry is missing | hostStats.rxBcastFrames stays zero when the PC sends the DHCP offer. | Confirm the EnetApp_addMCastEntry() function at test_enet.c:147 is called before the main_loop() function. |
| The state of the ALE port is not FORWARD | macStats.aleDrop or macStats.aleBlockDrop are incrementing. | Set the state of the MAC port and host port ALE to CPSW_ALE_PORTSTATE_FORWARD. |
| The host PC firewall is blocking DHCP | Packet capture on the PC shows DISCOVER is sent but the OFFER never leaves the interface. | Disable the Windows® and Linux® firewalls on the test Ethernet interface. |