SLUUDO2 September 2026 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
| Cause | How to Check | Fix |
|---|---|---|
| Loopback not enabled | Read the PHY control register, check bit 14 | Verify the PHY driver supports loopback. Check the PHY datasheet to verify the loopback register setting. |
| PHY reset during test | Check if the link LED on the PHY turns off | Verify the power stability of the PHY. |
| DMA RX not configured | Check if hRxCh is valid | Verify the DMA channel open succeeded. Check if the RX interrupts are enabled. Check the statistics to see if packets are reaching the host port. |
| RX buffer pool empty | Check if rxFreeQ has buffers | Verify LargePoolPktCount and MediumPoolPktCount in SYSCFG is adequate. |
| PHY clock domain isolation | Check the board schematic for clock routing | Potentially requires a PCB rework if not isolated properly. |