MAC Port Statistics – Counters
at the GMAC boundary:
- Count frames as seen on the wire, before ALE processing.
- rxGoodFrames increments when a valid Ethernet frame is received from the
PHY.
- Error counters (rxCrcErrors,
rxJabberFrames, and so forth) reflect the quality of the physical layer.
- The ALE drop counters within the
MAC block (aleDrop, portMaskDrop, and so forth) capture frames the ALE discards
on ingress from the MAC Port 1.
- The TX counters reflect frames
successfully placed on the wire.
Host Port Statistics – Counters
at the CPPI and DMA boundary:
- Count frames as seen by the CPU DMA interface, after ALE processing.
- rxGoodFrames increments when a frame is delivered to the DMA RX ring.
- txGoodFrames increments when a frame from the DMA TX ring exits the host
port.
- The ALE drop counters here
capture frames the ALE discards on ingress from the host port.
- The FIFO drop counters
(rxBottomOfFifoDrop and rxTopOfFifoDrop) reveal DMA back-pressure.